drAXIS#.IL.COGCOMP.TEACH.MOVE
Description
Runs the teach algorithm which makes a slow move, determines the effects of cogging, and then generates a cogging compensation table for the defined position range.
The axis must be enabled, in position mode, homed, and at the Teach Start Position before this command can be executed.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-08-00-000 |
General Information
|
Type |
Action |
|
Units |
N/A |
|
Range |
N/A |
| Default Value | N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL |
0x500A | 0x22 | UINT | 1:1 | - | W | False |
| AXIS2.IL.COGCOMP.TEACH.MOVE | 0x510A | 0x22 | UINT | 1:1 | - | W | False |